General Options (SP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The selection options for General Options are:

  • Outside Air Temperature: This option monitors the outdoor air temperature.

  • Outside Air Humidity: This option monitors the outdoor air humidity.

  • Mechanical Room Temperature: This option monitors the temperature of the mechanical room.