Basin Options (SP) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The selection options for Basin Options are:

  • Basin Level Alarm: This option monitors basin low level alarms.

  • Basin Heater Enable: This option generates BOs to command the basin heaters through the BAS.

  • Basin Water Temperature: This option monitors basin water temperatures.

    • Switch: This option monitors BI inputs for low temperature switches.

    • Analog Temperature: This option monitors AI inputs for temperature.

  • Basin Level Switch: This option monitors the basin levels.

  • Basin Makeup Valve: This option generates BOs to command basin makeup valves through the BAS.

If the No CW Piping (Air Cooled) node is selected, Basin Options cannot be selected.