Heating System Enable (CH) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The selection option for Heating System Enable is:

  • OA Heating Lockout: This option allows the system to be automatically enabled and disabled based on the outdoor air temperature.

  • Emergency Shutdown: This option allows the system to automatically shut down upon activation of a binary input.

  • Low Pressure Shutdown: This option allows the system to automatically shut down should the system pressure drop below a specified pressure.