No CW Piping (Air Cooled) (CPO) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Air-Cooled Condenser system does not use condenser water to cool the chillers, since they reject their heat by having ambient air passed across refrigerant-to-air heat exchangers. In packaged air-cooled chillers, the manufacturers attempt to provide optimal performance by staging fans in response to chiller load and ambient, dry-bulb temperature.