When you perform a box flow test, we recommend that you use certain starting positions. If you do not use the recommended starting positions, a message box appears that states the recommended starting positions, but you can still continue with the test. See the following table for the recommended starting positions.
System Type |
Recommendation |
---|---|
Single Duct with Exhaust |
Set the Exhaust box starting position the same as the Supply box starting position. |
Dual Duct |
Set the Hot deck starting position the opposite of the Cold deck starting position. |
Dual Duct with Exhaust |
Set the Hot deck starting position the same as the Cold deck starting position. Set the Exhaust box starting position the same as the Cold deck starting position. |