Mechanical System Selection - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This section corresponds to the mechanical selections available in the Mechanical System Selection screen of the System Selection Wizard. The Mechanical System Selection section is broken down into groups of selections based on how they appear in the wizard. Each group describes the selections available, any selection dependencies, and the modules that get laid down by the selections.

The modules are listed by type to identify where they appear in the Control View (for example, Network Inputs and Output Controllers). A category of modules is listed only if modules of that type are laid down by the particular group of selections, otherwise it is not included.