Analog Value Commands - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1 describes the Analog Value object commands. For information about command priorities, see Command Priority Levels.

Table 1. Analog Value Commands

Name

Description

Adjust

Releases priorities 9–15 and sets Priority 16 to the value you enter in the command. Present Value (appears as O1) changes to the highest value in the priority table.
Note: This command is available only if the Analog Value is prioritized.

Operator Override

Replaces Present Value (appears as O1) at the Operator Override priority with the value you enter in the command. The override has no effect if a higher priority value is in the Present Value attribute.
Note: This command is available only if the Analog Value is prioritized.

Release Operator Override

Releases an Operator Override command.
Note: This command is available only if the Analog Value is prioritized.

Release

Releases a specific priority of Present Value (appears as O1).
Note: This command is available only if the Analog Value is prioritized.

Release All

Releases Priorities 3–15.
Note: This command is available only if the Analog Value is prioritized.
Enable Alarms Enables all types of alarming.
Note: This command is available only if the Analog Value is prioritized.
Disable Alarms Disables all types of alarming.
Note: This command is available only if the Analog Value is prioritized.