Dehumidification Control (RTU) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
These selections provide the logic for dehumidification control.

The selection options for Dehumidification Control are:

  • Zone Humidity

  • Return Air Humidity

  • Activate Hot Gas Reheat during Dehumidification

Dehumidification cannot be selected unless both Cooling and Reheat are selected.