Configuration Options (MADD-MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
These selections allow the user to select the portion(s) of the Multizone logic to include in this system. The selection options are:

  • AHU Only

    • Zone Heating Valve Mode Output

    • Zone Staged Heating Mode Output

  • Zones Only

  • AHU + Zones