These selections provide the logic for determining the setpoints of the Cold Deck and Hot Deck temperature control loops. The Hot Deck Setpoint options apply only if a Hot Deck heating coil is selected.
The selection options for Temperature Control Strategy are:
-
Fixed Hot, Cold, or both Deck Temperatures
-
Hot, Cold, or both Deck Temperature Reset from OA-T
-
Hot Deck Temperature Reset from RA-T