Optional Equipment (MADD-MZ) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
These selections provide monitor-only sensors for an optional pre-filter, final filter, or both.

The selection options for Optional Equipment are:

  • Pre-Filter

    • Filter Switch

    • Filter Differential Pressure Sensor

  • Final Filter

    • Filter Switch

    • Filter Differential Pressure Sensor

  • Return Filter

    • Filter Switch

    • Filter Differential Pressure Sensor

These options are not applicable if the Zones Only configuration type is selected.