Zone Temperature (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Selecting this option adds an analog input for the zone temperature and uses this value in the primary temperature control loop. Additional options allow the user to select a Setpoint Adjust feature, which can be of either Common Setpoint Adjust or Warm Cool Adjust type, or a Temp Occ Support option to support a request for temporary occupancy from the zone sensor.