Summer and Winter Compensation Setpoint Shift (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Selecting this option shifts the heating and cooling setpoints to compensate for extreme outdoor air temperatures. This works similar to zone control reset by outdoor air temperature, with a large deadband so the setpoints are not modified while the outdoor air is between 50 and 75 °F.