Unoccupied Strategy (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
There are two choices for how the unit operates during unoccupied periods. Intermittent Night Operation cycles the fan as required to maintain the unoccupied heating and cooling setpoints. Off during Unoccupied turns the unit off.

Note: Heating, cooling, or both is not controlled during unoccupied operation. The required coils are operated at limited maximum output to drive the temperature to the unoccupied limit as quickly as possible.