Variable Speed Enthalpy Wheel (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This option adds a binary output and an analog output to control the heat wheel. Variable Speed enthalpy wheels rotate at a varying speed to control the temperature of the incoming air stream. If the minimum speed provides more heating or cooling than is necessary, an optional Bypass Damper BO can be energized to allow air to bypass the wheel.