Heat Recovery (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

This section defines an optional heat recovery device that exchanges heat between the exhaust air stream and the fresh air stream. These devices can be used for heating and cooling depending on the season.