Selecting the option for Fan Status adds a binary input for the toilet exhaust fan. You may select to restart the exhaust fan automatically or manually after the loss alarm is cleared. Selecting Manual Restart adds either a BI or Network Input to the system. This input must be commanded to restart the system.