Shutdown AHU When Pump is in Alarm (MASD) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
For applications with Preheat pumps, the Shutdown AHU when pump is in Alarm option prevents the unit from starting if there is a fault in the preheat pump during cold weather.