The next two sections define the type of cooling coil in the air handler. Staged cooling may be used for staged DX cooling coils. Staged DX coils always include the no flow lockout logic.
Device Rotation can be selected to rotate the first stage so that the stages get approximately equal runtime.
Number of Stages can be set from one to eight.