Modules (OADD Optional Sensors) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Optional Sensors selection loads the following modules in these Control View columns:

Network Inputs

  • OA-T (Outdoor Air Temperature): This module is loaded when a physical Outdoor Air Temperature input is not selected.

  • FLOW-LL (Airflow Low Limit): This module is loaded when Minimum Flow Protection For Staged Heating is selected. It is the minimum discharge flow required before staged heating is enabled.

See the Network Input Modules section.

Inputs

  • OA-T (Outdoor Air Temperature)

  • OA-H (Outdoor Air Humidity)

  • OA-Q (Outdoor Air Quality)

  • OA-VP (Outdoor Air Velocity Pressure)

  • OA-F (Outdoor Air Flow): The measurement is scaled using AI Output Range High.

  • PH-T (Preheat Temperature)

  • DA-H (Discharge Air Humidity)

  • DA-Q (Discharge Air Quality)

  • DA1-P (Discharge Air Static Pressure 1)

  • DA-VP (Discharge Air Velocity Pressure)

  • DA-F (Discharge Air Flow): The flow scaling is configured by setting the AI object’s Output Range High and Maximum Value attributes.

  • HD-T (Hot Deck Temperature)

  • HD-H (Hot Deck Humidity)

  • HD-P (Hot Deck Static Pressure)

  • HD-VP (Hot Deck Velocity Pressure)

  • HD-F (Hot Deck Flow): The flow scaling is configured by setting the AI object’s Output Range High and Maximum Value attributes.

  • CD-P (Cold Deck Static Pressure)

  • CD-VP (Cold Deck Velocity Pressure)

  • CD-F (Cold Deck Flow): The flow scaling is configured by setting the AI object’s Output Range High and Maximum Value attributes.

  • EA-T (Exhaust Air Temperature)

  • EA-H (Exhaust Air Humidity)

  • EA-Q (Exhaust Air Quality)

  • EA-P (Exhaust Air Static Pressure)

  • EA-VP (Exhaust Air Velocity Pressure)

  • EA-F (Exhaust Air Flow): The flow scaling is configured by setting the AI object’s Output Range High and Maximum Value attributes.

  • ZN-T (Zone Temperature)

  • ZN-H (Zone Humidity)

  • ZN-Q (Zone Quality)

  • BLDG-P (Building Static Pressure)

  • HR-T (Heat Recovery Temperature)

  • CLG-CL (Cooling Closed Status)
  • CLGFBD-POS (Cooling Face & Bypass Damper Position)
  • CLGFBD-S (Cooling Face & Bypass Damper Status)
  • CLG-OP (Cooling Open Status)
  • CLG-POS (Cooling Position)
  • CLG-S (Cooling Status)
  • HREAFBD-CL (Heat Recovery EA FBD Closed Status)
  • HREAFBD-OP (Heat Recovery EA FBD Open Status)
  • HREAFBD-POS (Heat Recovery EA FBD Position)
  • HREAFBD-S (Heat Recovery EA FBD Status)
  • HROAFBD-CL (Heat Recovery OA FBD Closed Status)
  • HROAFBD-OP (Heat Recovery OA FBD Open Status)
  • HROAFBD-POS (Heat Recovery OA FBD Position)
  • HROAFBD-S (Heat Recovery OA FBD Status)
  • HR-POS (Heat Recovery Position)
  • HR-S (Heat Recovery Status)
  • HTGX-POS (Heating X Position, where X is 1-2)
  • HTGX-S (Heating X Status, where X is 1-2)
  • HUM-S (Humidifier Status)
  • PHX-POS (Preheat X Position, where X is 1-2)
  • PHX-S (Preheat X Status, where X is 1-2)
  • PH-CL (Preheat Closed Status)
  • PHFBD-POS (Preheat Face & Bypass Damper Position)
  • PHFBD-S (Preheat Face & Bypass Damper Status)
  • PH-OP (Preheat Open Status)
  • PH-POS (Preheat Position)
  • PH-S (Preheat Status)
  • RH-POS (Reheat Position)
  • RH-S (Reheat Status)

See the Input Modules section.

Setpoint/Miscellaneous

State Generation