Modules (OADD Monitored Safeties) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Monitored Safeties selection loads the following modules in these Control View columns:

Inputs

  • DAPHI-A (Discharge Air High Duct Pressure)

  • DA-SD (Discharge Air Smoke Alarm)

  • EAPLO-A (Exhaust Air Low Duct Pressure)

  • EA-SD (Exhaust Air Smoke Alarm)

  • LT-A (Low Temperature Alarm)

  • HT-A (High Temperature Alarm)

  • HUMHI-A (Humidity High Limit)

See the Input Modules section.