Air Handling Unit Applications - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Air Handling Unit applications provide selections that are capable of controlling many different air handlers and control strategies. The selections for the AHU applications have Mechanical System and Control System options like other systems, but the selections are integrated together into the Mechanical System Selection section. Input sensors are automatically loaded if required for selected device or control options. The Control System Selection section provides optional sensors, equipment, and monitored safeties.