About this task
Note:
- The default installation is available if you want to accept all default options. If you want to customize your installation options, see the CCT custom installation and licensing section.
- All prerequisite software for CCT and the Software Manager are installed during the CCT installation process.
Procedure
- Obtain the product installation file.
- Run the JohnsonControlsControllerConfigurationTool_14.0.exe file. The Johnson Controls Controller Configuration Tool 14.0 Setup window appears.
- Click Install. All prerequisite software for CCT and the Software Manager are installed first, then the CCT software is installed.
- Click Finish when the Complete window appears.
-
Obtain field controller packages and SA Bus Device Packages to
install. To import a package, double-click on the package collection file or use
the Package Importer, located in the
Windows Start menu. The Package Importer displays the message
Finished importingwhen the import is complete. - To license CCT, run Software Manager from the Windows Start menu. Locate CCT in the Software Manager License Inventory and then click Activate New in the Choose Action menu. See Software Manager Help (LIT-12012389) for additional details on activating licenses.
-
To license field controller packages, run Software Manager from the Windows Start
menu. Use the Add License button in Software Manager if the field
controller package is not listed in the Software Manager License Inventory. If the
field controller package is listed in Software Manager, click Activate New in the
Choose Action menu. See Software Manager Help
(LIT-12012389) for additional details on activating licenses.
Note:
- Unlike CCT software, field controller package files are not automatically added to the Software Manager License Inventory when they are installed. Field controller packages are listed in Software Manager only after they have been initially licensed.
- If you do not license the CCT software after installation, the Software License Check appears when you access CCT for the first time. Field controllers without a licensed field controller package are set to Artificial Field Device or Artificial IO Device in CCT.
- Johnson Controls SA Bus Device Packages are included as a Feature within the CCT 14.x license. No additional action is necessary to license it after install.