Use this document to install or upgrade Controller Configuration Tool (CCT) software and field controller package files.
To order CCT software, specify the part number TL-CCT-0.
- If you have Metasys® CCT or Facility Explorer™ Programmable Configuration Tool (FX-PCT) Release 10.2 software or earlier installed on your computer, you must first uninstall it before installing CCT Release 10.3 or later. To determine what release you are using, go to in the tool. The release number is displayed next to Tool Version.
- If you have CCT or FX-PCT software at Release 10.3 installed on your computer, you can upgrade directly to CCT Release 13.0 or later.
- You are required to license both CCT software and field controller package files at Release 13.0 and later. For further information, see Installing and licensing the CCT software.
- At CCT 14.0, there is now a release mode 10.5 and release mode 10.3 is no longer included. For details about the different modes that are supported, refer to Controller Tool Help (LIT-12011147).
CCT provides the option to work within and switch between 10.2, 10.4 and 10.5 release modes. Refer to the User Interface section in the Controller Tool Help (LIT-12011147) for procedures. You can view Controller Application Files (CAFs) created at an earlier release of CCT or FX-PCT. If you want to edit these files, you need to upgrade them to an available release mode. For information on how to upgrade CAFs, refer to the Upgrading System Files section in Controller Tool Help (LIT-12011147) .