Controller Tool help - Johnson Controls - LIT-12011529 - Software Application - Controller Configuration Tool - 14.0

Controller Configuration Tool (CCT) Installation Instructions

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011529
Version
14.0
Revision date
2020-12-11
The Controller Tool Help (LIT-12011147) is the user’s guide to the CCT software. Use the Tool to configure, simulate, and commission the following:
  • Advanced Application Field Equipment Controllers (FACs)
  • Advanced Application Programmable Controllers (PCAs)
  • Expansion Input/Output Modules (PCXs)
  • Field Equipment Controllers (FECs)
  • General Purpose Application Controllers (CGMs)
  • General Purpose Programmable Controllers (PCGs)
  • Input/Output Modules (IOMs)
  • Programmable Variable Air Volume Box Controllers (PCVs)
  • SNC Series network engines
  • Variable Air Volume Controllers (VAVs)
  • Variable Air Volume Modular Assembly Controllers (VMAs)
  • Variable Air Volume Terminal Equipment Controllers (CVMs)
  • Expansion I/O Modules (XPMs)

The Controller Tool Help (LIT-12011147) provides guidance on communication switching, N2 point mapping, and N2 modules for N2 compatible controllers.