The
Controller Tool Help (LIT-12011147)
is the user’s guide to the CCT software. Use the Tool to configure,
simulate, and commission the following:
- Advanced Application Field Equipment Controllers (FACs)
- Advanced Application Programmable Controllers (PCAs)
- Expansion Input/Output Modules (PCXs)
- Field Equipment Controllers (FECs)
- General Purpose Application Controllers (CGMs)
- General Purpose Programmable Controllers (PCGs)
- Input/Output Modules (IOMs)
- Programmable Variable Air Volume Box Controllers (PCVs)
- SNC Series network engines
- Variable Air Volume Controllers (VAVs)
- Variable Air Volume Modular Assembly Controllers (VMAs)
- Variable Air Volume Terminal Equipment Controllers (CVMs)
- Expansion I/O Modules (XPMs)
The Controller Tool Help (LIT-12011147) provides guidance on communication switching, N2 point mapping, and N2 modules for N2 compatible controllers.