Overview - Johnson Controls - LIT-12013723 - CWPNLSNC1612-0 - CWPNLSNC2515-0 - Connected Workflow Turnkey Panel- M4-SNC Series Standard Control Panel Assembly

Connected Workflow Turnkey Panel - M4-SNC Series Standard Control Panel Assembly Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12013723
Revision date
2021-03-31

The Connected Workflow Turnkey Panel - Metasys® SNC Series Network Control Engine Standard Control Panel is a pre-wired and pre-assembled standard control panel that contains an SNC network engine. It also contains a cell modem, a remote antenna, and two antenna cables. This pre-configured solution saves time and money as it enables more efficient engineering, project management, commissioning, and customer closeout of projects.