Configuring initial connections - Johnson Controls - LIT-12013723 - CWPNLSNC1612-0 - CWPNLSNC2515-0 - Connected Workflow Turnkey Panel- M4-SNC Series Standard Control Panel Assembly

Connected Workflow Turnkey Panel - M4-SNC Series Standard Control Panel Assembly Quick Start Guide

Product
Document type
Quick Start Guide
Document number
LIT-12013723
Revision date
2021-03-31

Mounting the antenna

  1. Verify cell reception before you mount the antenna.
  2. Mount the antenna where cell reception is acceptable. You can mount the antenna on the panel or on a pole.
Note: You can use the 189 in. antenna cable to mount in a remote location. To mount the antenna outside the panel, the installer must provide a knock-out on the panel to pull the cabling through, and terminate to the modem inside the panel.
Figure 1. Antenna

Connecting the power

  1. Connect the cellular antenna to the WWAN PRI connector on the unit. If the unit is equipped with a secondary cellular antenna connector, connect it to the WWAN SEC connector.
  2. Connect 120 VAC power into the junction box at the top of the panel.
    Note: The panel requires 120 VAC power.

The project team receives specific directions from the remote operations center (ROC) about VPN set up, site-specific network assignments, and the relevant user name and password.