Changing the settings of the installed files for the CloudSync Service - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To change the settings of the installed files for the CloudSync Service, complete the following steps:

Procedure

  1. Navigate to C:/wwwcompanion/services/JCI.MyWorkplace.Integration.CloudSync/ JCI.MyWorkplace.Integration.CloudSync.exe.config
  2. In the Connection: Connection String section, modify the following settings:
  3. To connect to the database, replace the following information:
    • Replace [SQLServerInstance] with the SQL Server Instance name
    • Replace [DatabaseName] with Companion
    • Replace [Id] with the SQL Login user ID
    • Replace [Pwd] with the SQL Login password