CCure Service Installation - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To install the CCure Service, comeplete the following steps:

Procedure

  1. Open the installer package and select CompanionCCureService.msi.
  2. Double-click or right-click on the service to install the MSI. The MSI installs a windows service JCI.Companion.CCureService and creates a folder JCI.Companion.CCureService in the C drive.
  3. Modify the settings in C:\JCI.Companion.CCureService\ JCI.MyWorkplace.Integration.CCure.exe.config.
  4. In the Connection: Connection String section, modify the following settings:
  5. To connect to the database, replace the following information:
    • Replace [SQLServerInstance] with the SQL Server Instance name
    • Replace [DatabaseName] with Companion
    • Replace [Id] with the SQL Login user Id
    • Replace [Pwd] with the SQL Login password
  6. Modify the settings in C:\JCI.Companion.CCureService\ JCI.MyWorkplace.Integration.CCure.dll.config
  7. To connect to the database, replace the following information:
    • Replace [SQLServerInstance] with the SQL Server Instance name
    • Replace [DatabaseName] with Companion
    • Replace [Id] with the SQL Login user Id
    • Replace [Pwd] with the SQL Login password
  8. In the appSettings section, replace the following information:
    • BaseUrl – Replace [IP] with the IP Address of the CCure system
    • UserName – Replace [OperatorUserName] with the operator name for CCure
    • Password – Replace [OperatorPassword] with the password for the operator account
    • ClientName – Replace [ClientName] with the client name configured in CCure
    • Internal Api –Replace [InternalApiIP] with the IP address of the system where the internal API is installed (refer section 3.3)