Access Control System: Service Installation - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To install the P2000 service, complete the following steps:

Procedure

  1. Open the installer package and select CompanionP2000RmsService.msi.
  2. Double-click the MSI or right-click -> install for the file that you want to install. The MSI creates a Windows Service JCI.Companion.P2000RmsService and creates a folder JCI.Companion.P2000RmsService in the C drive.
  3. Navigate to C:\JCI.Companion.P2000RmsService\ JCI.MyWorkplace.IntegrationP2000RmsService.exe.config and, in the Connection: Connection String section, to connect to the database, replace the following information:
    • Replace [SQLServerInstance] with the SQL Server Instance name
    • Replace [DatabaseName] with Companion
    • Replace [Id] with the SQL Login user ID
    • Replace [Pwd] with the SQL Login password
  4. To connect to the P2000 database, replace the following information in the Pegasys Connection String:
    • Replace [P2000SQLServerInstance] with the SQL Server Instance name of the P2000 SQL Server
    • Replace [P2000Id] with the SQL Login user ID for the P2000 SQL Server
    • Replace [P2000Pwd] with the SQL Login password for the P2000 SQL Server
  5. In the appSettings section, change the port to the port number for integration with ACS. For further information, refer to appendix section 1. For the Internal API, replace [InternalApiIP] with the IP of the system on which the Internal API is installed (Refer section 3.3).