Installing IIS - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To enable and install IIS, complete the following steps:

Procedure

  1. From your computer desktop, navigate to Control Panel.
  2. Click Program, and then click Turn Windows Features On or Off.
  3. Click Add Roles or Features.
  4. From the sidebar, click Server Roles, then select the Web Server (IIS) check box.
  5. Click Add Features.
  6. Click Next repeatedly until you see the Role Services to install for Web Server (IIS) screen.
  7. From the CommonHttpFeatures section, select the StaticContent check box.
  8. From the Application Development section, in the Security section, select the ASP and ASP.NET 4.5 check boxes.
  9. Click Next and then click Install.

Results

IIS is enabled. You can check that IIS is enabled by searching for inetmgr from the Start menu on your computer. If IIS is enabled, you should see inetmgr in your results.