Installing .NET Core Runtime and Hosting Bundle - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To install the .NET Core Runtime and Hosting Bundle, complete the following steps:

Procedure

  1. From the installer package, click DotNet, and then click on the executable file: dotnethosting.exe.
  2. From the License Terms window, click Accept, and then click Install.
  3. Click Close when the installation is complete.

Results

To check if the bundle is installed, complete the following steps:
  1. From the Start menu on your computer, navigate to the Control Panel.
  2. Click Programs, and then click Uninstall Programs.
  3. From the list of installed programs, check for the following programs:
    • .Net Hosting Bundle
    • .Net Core Runtime

If you do not see the programs, the bundle is not installed. Therefore, you must repeat the installation process.