Changing the settings of the installed files for the WeatherRetriever Service - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To change the settings of the installed files for the WeatherRetriever service, complete the following steps:

Procedure

  1. Navigate to C:\services\servicescompanion\JCI.MyWorkplace.Integration.WeatherRetriever\ JCI.MyWorkplace.Integration.WeatherRetriever.exe.config.
  2. Navigate to the appSettings section and replace the value with the interval that you want the weather service to update in the application.
  3. Navigate to the connectionStrings section:

  4. To connect to the database, in the ConnectionString and MWPEntities section, replace the following information:
    • Replace [SQLServerInstance] with the SQL Server Instance name.
    • Replace [DatabaseName] with Companion.
    • Replace [Id] with the SQL Login user ID.
    • Replace [Pwd] with the SQL Login password.