Changing the settings of the installed files for the SwipeCommand Service - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To change the settings of the installed files for the SwipeCommand Service, complete the following steps:

Procedure

  1. Navigate to the following location: C:\services\servicescompanion\JCI.MyWorkplace.Integration.SwipeCommand\ JCI.MyWorkplace.Integration.SwipeCommand.exe.config.
  2. Navigate to the Connection: Connection String section:
  3. To connect to the database, replace the following information:
    • Replace [SQLServerInstance] with the SQL Server Instance name.
    • Replace [DatabaseName] with Companion.
    • Replace [Id] with the SQL Login user ID.
    • Replace [Pwd] with the SQL Login password.
  4. Navigate to the JCI.MyWorkplace.Integration.BMS.Core.dll.config section.
  5. In the appSettings section, replace the LightingCommandPriority and AirconCommandPriority with the required values or leave them as the default values.