Changing the settings of the installed files for the DataValidation Service - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To change the settings of the installed files for the DataValidation Service, complete the following steps:

Procedure

  1. Navigate to C:\services\servicescompanion\JCI.MyWorkplace.Integration.DataValidation\ JCI.MyWorkplace.Integration.DataValidation.exe.config.
  2. Navigate to the Connection: Connection String section.
  3. To connect to the database, replace the following information:
    • Replace [SQLServerInstance] with the SQL Server Instance name.
    • Replace [DatabaseName] with Companion.
    • Replace [Id] with the SQL Login user ID.
    • Replace [Pwd] with the SQL Login password.
  4. In the appSettings section, replace DV: Time with UTC time for the service to run and replace the following information:
    • [ClientId] – Replace the ClientId with the client ID of the web application registered in Azure AD under the organization’s tenant account.
    • [SecretKey] – Replace the SecretKey with the secret key of the web application registered in Azure AD under the organization’s tenant account.