Changing the settings of the installed files for the BookingCommand Service - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To change the settings of the installed files for the BookingCommand service, complete the following steps:

Procedure

  1. Navigate to the following location: C:\services\servicescompanion\JCI.MyWorkplace.Integration.BookingCommand\ JCI.MyWorkplace.Integration.BookingCommand.exe.config.
  2. Navigate to the Connection: Connection String section.
    To connect to the database, complete the following steps:
    • Replace [SQLServerInstance] with the SQL Server Instance name.
    • Replace [DatabaseName] with Companion.
    • Replace [Id] with the SQL Login user ID.
    • Replace [Pwd] with the SQL Login password.
  3. Navigate to the secureAppSettings section.
    Replace OutlookAdminEmail and OutlookAdminPassword with the POP3 account details.
  4. Navigate to the appSettings section.
    Replace OutlookExchangeURL with the Outlook Exchange URL.
  5. Navigate to JCI.MyWorkplace.Integration.BMS.Core.dll.config.
  6. Replace LightingCommandPriority and AirconCommandPriority with the required values or leave them as the default values.