Changing the settings for the Internal API files - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To change the settings for the installed files for the Internal API, complete the following steps:

Procedure

  1. From your computer, navigate to the path C:\wwwcompanioninternal\app.
  2. Double-click on the appsettings.json file.
  3. Navigate to the Connection: Connection String section:
    You must make the following changes to the section:
    • Replace [SQLServerInstance] with your SQL Server Instance name
    • Replace [DatabaseName] with the word Companion
    • Replace [Id] with your SQL Login User Id
    • Replace [Pwd] with your SQL Login Password
  4. In the case of P2000, navigate to the XmlRpcIntegration section:
    You must make the following changes to the section:
    • In the XmlRPcServiceEndpoint line, replace [IP] with the IP address of the P2000 server.
    • In the XmlRpcUserName line, replace [OperatorName] with the P2000 operator username.
    • In the XmlRpcPassword line, replace [OperatorPassword] with the P2000 password.
  5. In the case of CCure, navigate to the CCureIntegration section:
    You must make the following changes to the section:
    • In the UserName line, replace [OperatorName] with the Operator user name of CCure.
    • In the Password line, replace [OperatorPassword] with the password of the CCure Operator.
    • In the ClientName line, replace [ClientName] with the client name that is configured in CCure.
    • In the BaseUri line, replace [IP] with the IP address of the CCure Server.