Changing the settings for WCF Service files - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

About this task

To change the settings for the installed files for WCF Service, complete the following steps:

Procedure

  1. From your computer, navigate to the following location: C:\wwwcompanioninternal\BMSAPI.
  2. Double-click on the web.config file, and navigate to the Connection String section:
    You must make the following changes to the section:
    • Replace [SQLServerInstance] with the SQL Server Instance name.
    • Replace [DatabaseName] with the word Companion.
    • Replace [Id] with the SQL Login User ID.
    • Replace [Pwd] with the SQL Login Password.
  3. Navigate to the following location: C:\wwwcompanioninternal\BMSAPI\bin\.
  4. Double-click on the JCI.MyWorkplace.Integration.BMS.Core.dll.config file, and navigate to the appSettings section:
    You must make the following changes to the section:
    • Replace the LightingCommandPriority value with your required value, or leave it as the default value.
    • Replace the AirCommandPriority value with your required value, or leave it as the default value.