Order of Component installation - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

Use the following table to learn the order that each component must be installed.

Table 1. Components to be installed
Components External DMZ Internal DMZ Access Control System Order of installation
Database   Yes   1
CompanionInternal.msi   Yes   2
CompanionServices.msi   Yes   3
Companion.msi Yes     4
CompanionP2000RmsService.msi / CompanionCCureService.msi*     Yes 5
*Depending on the Access Control System of the facility, install either CompanionP2000RmsService.msi or CompanionCCureService.msi.