Installing the Companion application - Johnson Controls - LIT-12013270 - Software Application - Companion - 1.1

Companion Installation Guide

Brand
Johnson Controls
Product name
Companion
Document type
Installation Guide
Document number
LIT-12013270
Version
1.1
Revision date
2019-10-23
Language
English

Install the Companion Admin Portal application on to a computer running Windows Server 2012/2016. Install the Companion application either as a full installation or as a custom installation. When you apply changes in the Admin Portal, they display on all Companion mobile applications and on the Desk Reservation Kiosk.

Install the Companion application in the following ways:

  • Full installation: Install all modules of the Companion application.
  • Custom installation: Install individual modules of the Companion application.

Install and configure the Access Control System on the Access Control Server machine to ensure that there is an integration between the Companion application and the Access Control System.

Figure 1. Full Installation process
Figure 2. Custom Installation process