Trend log - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - Floating Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Proportional Fan Coil Thermostat - RTU Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Trend log
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 BACnet Object Identifier    
OBJECT_NAME     77 Character String    
OBJECT_TYPE     79 BACnet ObjectType    
ENABLE     133 BOOLEAN  
STOP_WHEN_FULL     144 BOOLEAN  
CLIENT_COV_INCREMENT     127 BACnet ClientCOV  
BUFFER_SIZE     126 Unsigned32    
LOG_BUFFER     131 BACnetLIST of BACnet LogRecord    
COV_RESUBSCRIPTION_INTERVAL     128 Unsigned Any value > 0
DESCRIPTION     28 Character String 40 characters max
LOG_DEVICEOBJECT_PROPERTY     132 BACnet Device Object Property Reference    
LOG_INTERVAL   1   134 Unsigned  
START_TIME     142 BACnet DateTime  
STOP_TIME     143 BACnet DateTime  
TRIGGER     205 BOOLEAN  
ACKED_TRANSITION   2          
EVENT_ENABLE   2   35 EventTransitionBits  
EVENT_TIME_STAMP   2   130 ARRAY[3] of BACnetTimeStamp    
LAST_NOTIFY_RECORD   2          
NOTIFICATION_CLASS   2   17 Unsigned 1–4,194,303
NOTIFICATION_THRESHOLD   2        
NOTIFY_TYPE   2   72 NotifyType  
RECORDS_SINCE_NOTIFICATION   2          
RECORD_COUNT     141 Unsigned32  
TOTAL_RECORD_COUNT     145 Unsigned32    
EVENT_STATE     36 EventState    
LOGGING_TYPE     197 LoggingType    
STATUS_FLAGS     111 StatusFlags    
RELIABILITY     103 Reliability    
ITEM_REFERENCE     32527 CharacterString    
USER_NAME     2390 CharacterString 400 characters max
STATUS     512 Enumerated    
ENABLED     673 Boolean  
EXECUTION_PRIORITY     2197 Enumerated 0–3
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
BUFFER_STATE     2565 Enumerated    
1 When entering Log_Interval or Sample_Interval times, only seconds can be entered even though the BACnet properties Log_Interval and Sample_Interval are in hundredths of a second. The value rounds down so if a value is entered for Log_Interval or Sample_Interval of 150, the resulting value is one second.
2 Only present when intrinsic alarming is enabled