Schedule - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - Floating Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Proportional Fan Coil Thermostat - RTU Thermostat - Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product name
Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Dynamically Creatable: Yes

Dynamically Deletable: Yes

Table 1. Schedule
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 BACnet Object Identifier    
OBJECT_NAME     77 Character String    
OBJECT_TYPE     79 BACnet ObjectType    
EFFECTIVE_PERIOD     32 BACnetDate Range  
LIST_OF_OBJECT_PROPERTY_REFERENCES     78 BACnetLIST of BACnet DeviceObject Property Reference  
OUT_OF_SERVICE     81 BOOLEAN  
PRESENT_VALUE     85 Any 1  
PRIORITY_FOR_WRITING     88 Unsigned (1..16)  
STATUS_FLAGS     111 BACnet StatusFlags    
RELIABILITY     103 BACnet Reliability    
SCHEDULE_DEFAULT     174 Any  
DESCRIPTION     28 Character String 40 characters max
EXCEPTION_SCHEDULE     38 BACnet ARRAY[N] of BACnet SpecialEvent  
WEEKLY_SCHEDULE     123 BACnet ARRAY[7] of BACnet Daily Schedule  
ITEM_REFERENCE     32527 CharacterString    
USER_NAME     2390 CharacterString 400 characters max
STATUS     512 Enumerated    
ENABLED     673 Boolean  
EXECUTION_PRIORITY     2197 Enumerated 0–3
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
1 Writable when OUT_OF_SERVICE is true.