Multistate value - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - RTU Thermostat - Floating Fan Coil Thermostat - Proportional Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Multistate value
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 BACnet Object Identifier    
OBJECT_NAME     77 Character String    
OBJECT_TYPE     79 BACnet Object Type    
NUMBER_OF_STATES     74 Unsigned   2–500
PRESENT_VALUE     85 Unsigned  
PRIORITY_ARRAY   1          
DESCRIPTION     28 Character String 40 characters max
STATUS_FLAGS     111 BACnet Status Flags    
EVENT_STATE     36 BACnet Event State    
RELIABILITY     103 BACnet Reliability 1  
OUT_OF_SERVICE     81 BOOLEAN    
RELINQUISH_DEFAULT   1        
STATE_TEXT     110 BACnet ARRAY[N] of Character String  
ACKED_TRANSITIONS   2   0 BACnet Event Transition Bits    
ALARM_VALUES   2   7 Unsigned 0–65,535
EVENT_ENABLE   2   35 BACnet Event Transition Bits  
EVENT_TIME_STAMPS   2   130 BACnet ARRAY[3] of BACnet Time Stamp    
EVENT_MESSAGE_TEXTS     351 BACnet ARRAY[3] of Character String    
FAULT_VALUES   2   39 Unsigned 0–65,535
NOTIFICATION_CLASS   2   17 Unsigned 1–4,194,303
NOTIFY_TYPE   2   72 BACnet NotifyType  
TIME_DELAY   2   113 Unsigned 0–65,535
ITEM_REFERENCE     32527 CharacterString    
USER_NAME     2390 CharacterString 400 characters max
STATUS     512 Enumerated    
ENABLED     673 Boolean  
EXECUTION_PRIORITY     2197 Enumerated 0–3
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
RESTORE_COMMAND_PRIORITY     721 Bit String  
OFFLINE     913 Boolean    
STATES_TEXT     931 Enumerated    
INTRINSIC_ALARMING_DEFINED     569 Boolean  
GRAPHIC     2 32581 CharacterString  
GRAPHIC_ALIAS     2 32623 CharacterString  
ALARM_MESSAGE_TEXT     2 536 CharacterString  
1 Not present in all instances.
2 Only present when intrinsic alarming is enabled.