File - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - RTU Thermostat - Floating Fan Coil Thermostat - Proportional Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document number
LIT-12013203
Revision date
2020-05-21
Note: File objects can only be modified by replacing the entire file.
Note: File objects must be written sequentially.

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. File
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 BACnetObject Identifier    
OBJECT_NAME     77 CharacterString    
OBJECT_TYPE     79 BACnetObject Type    
ARCHIVE     13 BOOLEAN  
FILE_SIZE 1     42 Unsigned  
DESCRIPTION     28 CharacterString 40 characters max
FILE_TYPE     43 Character String    
MODIFICATION_DATE     71 BACnetDateTime    
READ_ONLY     99 BOOLEAN    
FILE_ACCESS_METHOD     41 BACnetFile AccessMethod    
ITEM_REFERENCE     32527 CharacterString    
USER_NAME     2390 CharacterString 400 characters max
STATUS     512 Enumerated    
ENABLED     673 Boolean  
EXECUTION_PRIORITY     2197 Enumerated 0–3
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
MAX_FILE_SIZE     3380 Unsigned    
1 Can write zero (0) to file size but arbitrary truncation or expansion is not supported.