Dynamically Creatable: No
Dynamically Deletable: No
| Property name | Required | Optional | Proprietary | Property ID | Data type | Writable | Range |
|---|---|---|---|---|---|---|---|
| OBJECT_IDENTIFIER | √ | 75 | ObjectIdentifier | ||||
| OBJECT_NAME | √ | 77 | CharacterString | ||||
| OBJECT_TYPE | √ | 797 | ObjectType | ||||
| OUT_OF_SERVICE | √ | 81 | BOOLEAN | √ | |||
| PRESENT_VALUE | √ | 85 | BinaryPV | √ | |||
| RELINQUISH_DEFAULT | √ | 104 | BinaryPV | √ | |||
| COS_COUNT | √ | 15 | Unsigned | √ | |||
| DESCRIPTION | √ | 28 | CharacterString | √ | 40 characters max | ||
| DEVICE_TYPE | √ | 31 | CharacterString | √ | 20 characters max | ||
| STATUS_FLAGS | √ | 111 | StatusFlags | ||||
| EVENT_STATE | √ | 36 | EventState | ||||
| ELAPSED_ACTIVE_TIME | √ | 33 | Unsigned32 | √ | |||
| MIN_OFF_TIME | √ | 66 | Unsigned32 | √ | |||
| MIN_ON_TIME | √ | 67 | Unsigned32 | √ | |||
| RELIABILITY | √ | 103 | Reliability | √ | |||
| POLARITY | √ | 84 | Polarity | √ | |||
| INACTIVE_TEXT | √ | 46 | CharacterString | √ | |||
| ACTIVE_TEXT | √ | 4 | CharacterString | √ | |||
| CHANGE_OF_STATE_TIME | √ | ||||||
| CHANGE_OF_STATE_COUNT | √ | ||||||
| TIME_OF_ACTIVE_TIME_RESET | √ | ||||||
| COS_TIME | √ | 16 | DateTime | ||||
| INACTIVE_TEXT | √ | 46 | CharacterString | ||||
| TIME_OF_STATE_COUNT_RESET | √ | ||||||
| PRIORITY_ARRAY | √ | 87 | PriorityArray | ||||
| EVENT_MESSAGE_TEXTS | √ | 351 | ARRAY[3] of CharacterString | ||||
| ACKED_TRANSITIONS | √ 1 | ||||||
| EVENT_ENABLE | √ 1 | 35 | EventTransitionBits | √ | |||
| EVENT_TIME_STAMPS | √ 1 | 130 | ARRAY[3] of BACnetTimeStamp | ||||
| NOTIFICATION_CLASS | √ 1 | 17 | Unsigned | √ | 1–4,194,303 | ||
| NOTIFY_TYPE | √ 1 | 72 | NotifyType | √ | |||
| FEEDBACK_VALUE | √ 1 | 40 | BinaryPV | √ | |||
| TIME_DELAY | √ 1 | 113 | Unsigned | √ | 0–65,535 | ||
| ITEM_REFERENCE | √ | 32527 | CharacterString | ||||
| USER_NAME | √ | 2390 | CharacterString | √ | 400 characters max | ||
| STATUS | √ | 512 | Enumerated | ||||
| ENABLED | √ | 673 | Boolean | √ | |||
| EXECUTION_PRIORITY | √ | 2197 | Enumerated | √ | 0–3 | ||
| OBJECT_CATEGORY | √ | 908 | Enumerated | √ | 0–111 | ||
| ALARM_STATE | √ | 1006 | Enumerated | ||||
| INSTANCE_NUMBER | √ | 32589 | Unsigned | ||||
| TRUNK_NUMBER | √ | 549 | Unsigned | ||||
| DEVICE_MAC_ADDRESS | √ | 3629 | Unsigned | ||||
| OFFLINE | √ | 913 | Boolean | ||||
| IN_TEST | √ | 3368 | Boolean | ||||
| COV_COUNT | √ | 839 | Unsigned | ||||
| HEAVY_EQUIP_DELAY | √ | 516 | Unsigned | √ | |||
| HED_CONTROLLER | √ | 517 | Unsigned | √ | |||
| STATES_TEXT | √ | 931 | Enumerated | ||||
| INTRINSIC_ALARMING_DEFINED | √ | 569 | Boolean | √ | |||
| SAB_MAC_ADDR | √ | 3645 | Unsigned | ||||
| SLOT_A | √ | 990 | Unsigned | ||||
| SLOT_B | √ | 991 | Unsigned |
1 Only present when intrinsic alarming is
enabled.