Binary output - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - RTU Thermostat - Floating Fan Coil Thermostat - Proportional Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Binary output
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 ObjectIdentifier    
OBJECT_NAME     77 CharacterString    
OBJECT_TYPE     797 ObjectType    
OUT_OF_SERVICE     81 BOOLEAN  
PRESENT_VALUE     85 BinaryPV  
RELINQUISH_DEFAULT     104 BinaryPV  
COS_COUNT     15 Unsigned  
DESCRIPTION     28 CharacterString 40 characters max
DEVICE_TYPE     31 CharacterString 20 characters max
STATUS_FLAGS     111 StatusFlags    
EVENT_STATE     36 EventState    
ELAPSED_ACTIVE_TIME     33 Unsigned32  
MIN_OFF_TIME     66 Unsigned32  
MIN_ON_TIME     67 Unsigned32  
RELIABILITY     103 Reliability  
POLARITY     84 Polarity  
INACTIVE_TEXT     46 CharacterString  
ACTIVE_TEXT     4 CharacterString  
CHANGE_OF_STATE_TIME            
CHANGE_OF_STATE_COUNT            
TIME_OF_ACTIVE_TIME_RESET            
COS_TIME     16 DateTime    
INACTIVE_TEXT     46 CharacterString    
TIME_OF_STATE_COUNT_RESET            
PRIORITY_ARRAY     87 PriorityArray    
EVENT_MESSAGE_TEXTS     351 ARRAY[3] of CharacterString    
ACKED_TRANSITIONS   1          
EVENT_ENABLE   1   35 EventTransitionBits  
EVENT_TIME_STAMPS   1   130 ARRAY[3] of BACnetTimeStamp    
NOTIFICATION_CLASS   1   17 Unsigned 1–4,194,303
NOTIFY_TYPE   1   72 NotifyType  
FEEDBACK_VALUE   1   40 BinaryPV  
TIME_DELAY   1   113 Unsigned 0–65,535
ITEM_REFERENCE     32527 CharacterString    
USER_NAME     2390 CharacterString 400 characters max
STATUS     512 Enumerated    
ENABLED     673 Boolean  
EXECUTION_PRIORITY     2197 Enumerated 0–3
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
INSTANCE_NUMBER     32589 Unsigned    
TRUNK_NUMBER     549 Unsigned    
DEVICE_MAC_ADDRESS     3629 Unsigned    
OFFLINE     913 Boolean    
IN_TEST     3368 Boolean    
COV_COUNT     839 Unsigned    
HEAVY_EQUIP_DELAY     516 Unsigned  
HED_CONTROLLER     517 Unsigned  
STATES_TEXT     931 Enumerated    
INTRINSIC_ALARMING_DEFINED     569 Boolean  
SAB_MAC_ADDR     3645 Unsigned    
SLOT_A     990 Unsigned    
SLOT_B     991 Unsigned    
1 Only present when intrinsic alarming is enabled.