Binary input - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - Floating Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Proportional Fan Coil Thermostat - RTU Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Binary input
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 ObjectIdentifier    
OBJECT_NAME     77 CharacterString    
OBJECT_TYPE     797 ObjectType    
PRESENT_VALUE     85 BinaryPV  
OUT_OF_SERVICE     81 BOOLEAN  
COS_COUNT     15 Unsigned  
DESCRIPTION     28 CharacterString   40 characters max
DEVICE_TYPE     31 CharacterString   20 characters max
STATUS_FLAGS     111 StatusFlags    
EVENT_STATE     36 EventState    
POLARITY     84 Polarity    
INACTIVE_TEXT     46 CharacterString  
ACTIVE_TEXT     4 CharacterString  
CHANGE_OF_STATE_TIME            
CHANGE_OF_STATE_COUNT          
TIME_OF_STATE_COUNT_RESET            
ELAPSED_ACTIVE_TIME     33 Unsigned32  
TIME_OF_ACTIVE_TIME_RESET            
RELIABILITY     103 Reliability  
ACTIVE_TEXT            
ACTIVE_TIME_RESET     114      
COS_TIME     16      
INACTIVE_TEXT     46 CharacterString    
STATE_COUNT_RESET     115      
ACKED_TRANSITIONS   1          
ALARM_VALUES   1   7 BinaryPV  
EVENT_ENABLE   1   35 EventTransitionBits  
EVENT_TIME_STAMPS   1   130 ARRAY[3] of BACnetTimeStamp    
EVENT_MESSAGE_TEXTS     351 ARRAY[3] of CharacterString    
NOTIFICATION_CLASS   1   17 Unsigned 1–4,194,303
NOTIFY_TYPE   1   72 NotifyType  
TIME_DELAY   1   113 Unsigned 0–65,535
ITEM_REFERENCE     32527 CharacterString    
USER_NAME     2390 CharacterString 400 characters max
STATUS     512 Enumerated    
ENABLED     673 Boolean  
EXECUTION_PRIORITY     2197 Enumerated 0–3
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
INSTANCE_NUMBER     32589 Unsigned    
TRUNK_NUMBER     549 Unsigned    
DEVICE_MAC_ADDRESS     3629 Unsigned    
OFFLINE     913 Boolean    
IN_TEST     3368 Boolean    
COV_COUNT     839 Unsigned    
STATES_TEXT     931 Enumerated    
INTRINSIC_ALARMING_DEFINED     569 Boolean  
SAB_MAC_ADDRS     3645 Unsigned    
1 Only present when intrinsic alarming is enabled.