Analog value - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - RTU Thermostat - Floating Fan Coil Thermostat - Proportional Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Analog value
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 BACnetObject Identifier    
OBJECT_NAME     77 CharacterString    
OBJECT_TYPE     79 BACnetObject Type    
PRESENT_VALUE     85 REAL  
UNITS     117 BACnet Engineering Units 0–65,535
PRIORITY_ARRAY   1          
COV_INCREMENT     22 REAL 2 any value > 0
DESCRIPTION     28 Character String 40 characters max
STATUS_FLAGS     111 BACnetStatusFlags    
EVENT_STATE     36 BACnetEventState    
RELIABILITY     103 BACnet Reliability  
OUT_OF_SERVICE     81 BOOLEAN    
ACKED_TRANSITIONS   3   0 BACnetEvent TransitionBits    
DEADBAND   3   25 REAL  
EVENT_ENABLE   3   35 BACnetEvent TransitionBits  
EVENT_TIME_STAMPS   3   130 BACnet ARRAY[3] of BACnet TimeSTamp    
EVENT_MESSAGE_TEXTS     351 BACnet ARRAY[3] of Character String    
HIGH_LIMIT   3   45 REAL  
LIMIT_ENABLE   3   52 BACnetLimit Enable  
LOW_LIMIT   3   59 REAL  
NOTIFICATION_CLASS   3   17 Unsigned 1–4,194,303
NOTIFY_TYPE   3   72 BACnet NotifyType  
TIME_DELAY   3   113 Unsigned 0–65,535
ITEM_REFERENCE     32527 CharacterString    
STATUS     512 Enumerated    
ENABLED     673 Boolean  
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
RESTORE_COMMAND_PRIORITY     721 Bit String  
INTRINSIC_ALARMING_DEFINED     569 Boolean  
OFFLINE     913 Boolean    
MAX_PRES_VALUE     65 Real  
MIN_PRES_VALUE     69 Real  
USE_COV_MIN_SEND_TIME     1 3930 Boolean  
1 Not present in all instances.
2 Not writable in all instances.
3 Only present when intrinsic alarming is enabled.