Analog output - Johnson Controls - LIT-12013203 - TEC36xx-10-000 - Floating Fan Coil Thermostat - Heat Pump Thermostat - On/Off Fan Coil Thermostat - Proportional Fan Coil Thermostat - RTU Thermostat - Color Terminal Equipment Controller

Color Terminal Equipment Controller (TEC) Protocol Implementation Conformance Statement

Product
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013203
Revision date
2020-05-21

Dynamically Creatable: No

Dynamically Deletable: No

Table 1. Analog output
Property name Required Optional Proprietary Property ID Data type Writable Range
OBJECT_IDENTIFIER     75 ObjectIdentifier    
OBJECT_NAME     77 CharacterString    
OBJECT_TYPE     79 ObjectType    
DEVICE_TYPE     31 CharacterString    
STATUS_FLAGS     111 StatusFlags    
EVENT_STATE     36 EventState    
OUT_OF_SERVICE     81 BOOLEAN  
PRESENT_VALUE     85 REAL  
RELINQUISH_DEFAULT     104 REAL  
UNITS     117 EngineeringUnits 0–65,535
COV_INCREMENT     22 REAL any value > 0
DESCRIPTION     28 CharacterString 40 characters max
OBJECT_TYPE     797 ObjectType   20 characters max
MAX_PRES_VALUE     65 REAL  
MIN_PRES_VALUE     69 REAL  
RELIABILITY     103 Reliability    
RESOLUTION     106 REAL    
PRIORITY_ARRAY     87 PriorityArray    
EVENT_MESSAGE_TEXTS     351 ARRAY[3] of CharacterString    
ACKED_TRANSITIONS   1          
DEADBAND   1   2205 REAL  
EVENT_ENABLE   1   35 EventTransitionBits  
EVENT_TIME_STAMPS   1   130 ARRAY[3] of BACnetTimeStamp    
HIGH_LIMIT   1   45 REAL  
LIMIT_ENABLE   1   52 LimitEnable  
LOW_LIMIT   1   59 REAL  
NOTIFICATION_CLASS   1   17 Unsigned 1–4,194,303
NOTIFY_TYPE   1   72 NotifyType  
TIME_DELAY   1   113 Unsigned 0–65,535
ITEM_REFERENCE     32527 CharacterString    
USER_NAME     2390 CharacterString 400 characters max
STATUS     512 Enumerated    
ENABLED     673 Boolean  
EXECUTION_PRIORITY     2197 Enumerated 0–3
OBJECT_CATEGORY     908 Enumerated 0–111
ALARM_STATE     1006 Enumerated    
OFFLINE     913 Boolean    
DISPLAY_PRECISION     661 Enumerated 0–12
INTRINSIC_ALARMING_DEFINED     569 Boolean  
SAB_MAC_ADDR     3645 Unsigned    
SLOT_A     990 Unsigned    
USE_COV_MIN_SEND_TIME     3930 Boolean  
RESTORE_COMMAND_PRIORITY     721 Bit String  
1 Only present when intrinsic alarming is enabled.